Browse FAQs

Osisense XC - Cross of the obsolete XCKJ561H7 limit switch

Published date: 14 May 2019

The obsolete XCKJ561H7 limit switch reference is no more available in 2019 as a complete limit switch. It has to be ordered by the sub-assemblies ZCKJ5H7 body + ZCKE61 metal end plunger. Alternative is to select XCKJ part number with another cable entry like the XCKJ561 (cable entry Pg 13.5) or XCKJ561H29 (cable entry ISO M20)


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.