Browse FAQs

Osisense XC - Cross of the XCKJ50513H7 limit switch

Published date: 12 June 2019

The XCKJ50513H7 limit switch reference is no more available in 2019 as a complete limit switch. It has to be ordered by the sub-assemblies ZCKJ5H7 body + ZCKE05 rotary head + ZCKY13 steel roller lever. Alternative is to select XCKJ part number with another cable entry like the XCKJ50513H29 with ISO M20 cable entry


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.