Browse FAQs

Osisense XC - is XCKJ108 commercialized?

Published date: 12 June 2019

The complete switch XCKJ108 is not commercialized in 2019. Customer who needs it, has to order it under the following sub-assemblies ZCKJ1 contact body + ZCKE08 spring head. Part number XCKJ108H29 is available to order in 2019 (sub-assemblies ZCKJ1H29 + ZCKE08)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.