Browse FAQs

TCP Ports used internally by Modbus Driver Suite

Published date: 13 May 2019

Title
Modbus Driver Suite used TCP ports
 
Issue
List of the TCP Ports used internally by Modbus Driver Suite
 
Product Line
Modbus Driver Suite
 
Environment
Windows Operating Systems
 
Resolution
The following ports are identified to be associated with the Modbus drivers as noted.
Windows sockets are used as interface between application and SE-communication drivers.
The following code excerpt shows, which ports are associated to the various SE-communication channels

Channel            Port(s)
MBS01              27700
MBS02              27701
MBS03              27702

MBP01              27710 & 27711
MBP02              27712 & 27713

UNTLW01            27720 & 27721
UNTLW02            27722 & 27723
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.