Browse FAQs

Preventa XY2C - Do we have an XY2CZ cable dia 5mm longer than the XY2CZ310 100.5m length

Published date: 03 June 2019

The XY2CZ310 is the red cable dia 5mm 100.5m length. For OEM need and higher length, we can suggest the following part numbers
- XY2CZ125 = 250m in 1 cable reel
- XY2CZ125TQ = 250m x 8 cable reels (see attached picture)
Both references are available to order in 2019

Was this helpful?

What can we do to improve the information ?