Browse FAQs

Osisense XC - XCMN21**L1 basic limit switches - Why 2 rings are supplied in the product packaging

Published date: 03 May 2019

Attached XCMN2102L1 complete plastic bag supplied at delivery. It shows 2 ring supplied in a liitle bag.
Q) Why are they supplied?
A) They need to be mounted in the plastic enclosure holes to reinforce the case when the fixing screws are tightened. See attached picture showing the rings mounted. It is difficult to remove them after the assembling

Was this helpful?

What can we do to improve the information ?