Browse FAQs

How to print a SoMachine project?

Published date: 03 April 2019

Issue:
How to print a SoMachine project?

Product Line:
SoMachine

Resolution:
Possible reasons of the A320 error are:
1. Higher amount of friction in application that is on this motor - check the mechanical if there is some blockage, check bearing.
2. Gearbox attached on the motor has higher friction because it lost lubrication

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.