Browse FAQs

Is it possible to use the HMIDMA521 a separate monitor?

Published date: 29 March 2019

Issue:
Is it possible to use the HMIDMA521 a separate monitor?

Product Line:
Magelis HMIDM series

Resolution:
In order to use the HMIDMA521 as a separate display (without an iPC), you will need to attach the HMIDADP11 display adaptor and connect to the Display Port input from your PC source output.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.