Browse FAQs

How can I check on the motor speed on the ATV212 drive?

Published date: 08 April 2019

Issue:
How can I check on the motor speed on the ATV212 drive?

Product Line:
Altivar ATV212

Environment:
All serial numbers

Cause:
Customer wanted to know how to check the actual motor speed on the drive.

Resolution:
Using the integral keypad, push the MODE button until you see Fr-F.  Do not Push ENTER, scroll down until you see 1500.  In this case, 1500 is the motor speed in RPM.  Please see the attachment below for more details.



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.