Browse FAQs

How do I mitigate security vulnerabilities with the 174CEV20040

Published date: 29 March 2019

 I have found that a DMDI announcing an end-of-sales date of 12/31/15,  and an end-of-service date of 12/31/2018 was issued on 11/25/2014.  Therefore, there is no longer any support offered on this product.  There are however, recommendations made as part of this attached DMDI that are available through the Schneider Electric CAPP partners program.  I suggest the customer consider these products as part of his mitigation strategy.  Another option would be to put the current product behind a firewall that would provide the protection necessary to mitigate the identified vulnerabilities.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.