Browse FAQs

Is the ATV212 capable of ramp switching?

Published date: 16 September 2019

Issue:
INeeds the  ramp switching function on the ATV212. 

Product Line:
Altivar 212

Environment:
All

Cause:
Functionality question

Resolution:
Yes, the ATV212 has ramp switching functionality. This is done with the F504 parameter. Please see the ATV212 Programming Manual for further details.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.