Browse FAQs

Osisense XC - Composition of the XCKP2149M12 limit switch with M12 4-pin connector

Published date: 20 March 2019

The XCKP2149M12 limit switch with M12 4-pin connector is available to order in 2019. It's made of the following sub-assemblies: ZCP21M12 body + ZCE01 head + ZCY49 dia50mm roller lever

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.