Browse FAQs

How to set up "Automatic Start in Run" using EcoStruxure Control Expert (formally known as Unity Pro)..

Published date: 15 April 2019

Issue:
How to configure start in run using EcoStruxure Control Expert software.

Product line:
All M340, M580 and Unity Momentum Processors

Environment:
ExoStruxure Control Expert, ( formally Unity Pro).

Cause:
If not set on power cycle controller will not come up in run mode.

Resolution:
Open or create project
Select PLC Model, part number and version
Open configuration and PLC bus and double click on the PLC.
The configuration tab opens you will see the options and select "Automatic Start in Run" and save.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.