Browse FAQs

Max number for Comm Port in SoMove

Published date: 19 March 2019

Issue:
What is the maximum number you can use in the COM port setting after which SoMove does not work?

Product Line:
ATV6XX, ATV9XX

Environment:
All

Cause:
NA

Resolution:
There is no such limit.
SoMove detects all the COM's active on your PC and works fine even with COM256 (max.number for Win10)

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.