Browse FAQs

Can the ATV312 be 'line started'?

Published date: 19 March 2019

Issue:
Can the ATV312 be 'line started'? 

Product Line:
Altivar 312

Environment:
All

Cause:
Wiring and programming the ATV312 to run automatically when line voltage is supplied 

Resolution:
Yes, the ATV312 can be set up to run this way. The drive must be set to 2-wire control (2C) for this setup.

Note: This is in addition to basic programming, including programming the drive for your motor. 

Programming:
tCC= 2C
tCt= LEL 

Wiring:
Jumper +24V to LI1

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.