Browse FAQs

What are the SD card options for the M340 Processor?

Published date: 15 March 2019

Issue:
Types of SD cards available for the M340 Processors

Product line:
M340 Processors

Environment:
EcoStruxure Control Expert ( formally known as Unity Pro)

Resolution:
The compatibility of the two memory cards is as follows:
 BMX RMS 008MP card compatible with all processors.
 BMX RMS 008MPF and BMX RMS 128MPF cards compatible with the following processors:
 BMX P34 2000,
 BMX P34 2010,
 BMX P34 20102,
 BMX P34 2020,
 BMX P34 2030,
 BMX P34 20302.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.