Browse FAQs

What are the EcoStruxure Machine Expert – Basic system requirements?

Published date: 12 March 2019

This software can be installed on a personal computer having the following hardware:
  • Processor                Core 2 duo or better
  • RAM Memory           2 GBytes or greater
  • Hard Disk                600 MBytes
  • Display                    1280 x 768 pixels resolution or better
  • Peripherals               Mouse or compatible pointing device
  • Peripherals               USB interface
  • Web access             Web registration requires Internet access
 
Supported operating systems:
  • Microsoft Windows 10
  • Microsoft Windows 8.1 Professional Edition 32 Bit & 64 Bit
  • Microsoft Windows 8 Professional Edition 32 Bit & 64 Bit
  • Microsoft Windows 7 Professional Edition 32 Bit & 64 Bit
 
Machine Expert – Basic requires Administrator rights to be installed.
Remove any USB connection to the controller when installing or uninstalling Machine Expert – Basic.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.