Browse FAQs

Can I setup monitor parameters for the pump on the ATV12?

Published date: 22 March 2019

Issue:
Can I setup monitor parameters for the pump on the ATV12?

Product Line:
Altivar ATV12

Environment:
All serial numbers

Cause:
Customer wanted to know if he can monitor the pellet jammed up before it happened. 

Resolution:
The drive does not have the function to monitor the jam up in the Pellet.  However, if customer uses PLC with the drive, then customer can find out what are the registers to monitor motor current, motor voltage, output power to check when the jam up in the Pellet occurred.

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.