Browse FAQs

Can the ATV212HU22M3X be used with 480V input power supply?

Published date: 22 March 2019

Issue:
Can the ATV212HU22M3X be used with 480V input power supply?

Product Line:
Altivar ATV212

Environment:
All serial numbers

Cause:
Customer only had 480V input power supply.

Resolution:
The ATV212HU22M3X has suffix "M3" and therefore it is rated for 208-240V 3 phase input only.  It cannot be used with the 480V input power supply.   

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.