Browse FAQs

How do we use the Square Root Function in Vijeo Designer?

Published date: 06 March 2019

Issue:
How do we use the Square Root Function in Vijeo Designer?

Product Line:
Vijeo Designer (all versions)

Resolution:
To use the Square Root Function in Vijeo Designer, you must use it in an expression editor. In otherwords, for any object that is able to handle expressions, you can use the function

To use the function, type the following "sqrt(VariableName)"

This will display the Square Root value of "VariableName"

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.