Browse FAQs

How do I connect to a SoMachine controller though EcoStruxure Secure Connect Advisor?

Published date: 05 March 2019

Issue:
The EcoStruxure Secure Connect Advisor allows to connect to the controller remotely through a VPN connection.

Product Line:
M241
M251
LMC058

Environment:
SoMachine V4.3

Resolution:

1) Establish the VPN connection with EcoStruxure Secure Connect Advisor.
2) Test the connecting with a Ping command to the PLC.
4) Double click on the controller under the device tree.  Under the Controller selection select  IP Address via NAT (Remote TCP)
5) Enter the IPaddress of the PLC under NAT Address and Target IP address.  The port is usually 1105.
 


Was this helpful?

What can we do to improve the information ?