Browse FAQs

What is the voltage for the start and stop on the ATS48?

Published date: 05 March 2019

Issue:
Control voltage for the start and stop on the ATS48 soft start.

Product Line:
Altistart 48

Environment:
All

Cause:
Documentation

Resolution:
The control power is 24 volts. The +24V terminal is a 24 VDC source.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.