Browse FAQs

When installing Unity Pro, I see "Could not register C:\Windows\SysWOW64\OEM FDT Container.dll". How can this be resolved?

Published date: 01 March 2019

Issue
When installing Unity Pro, I see "Could not register C:\Windows\SysWOW64\OEM FDT Container.dll". How can this be resolved?
 
Product Line
Unity Pro
 
Environment
Windows PC
 
Cause
This is caused by the C:\Windows\SysWOW64\OEM FDT Container.dll file already pre-existing with a different product's installation and the Unity Pro installer cannot register it.
 
Resolution
The dll file can be registered manually from the Windows command (cmd) line.
1) Run Windows Command Line as Administrator
2) Type the command: regsvr32 "C:\Windows\SysWOW64\OEM FDT Container.dll"
3) Press enter

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.