Browse FAQs

What is the part number of the UV protection sheet for the Magelis HMIGTO2300, HMIGTO2310, and HMIGTO2315?

Published date: 01 March 2019

Issue
What is the part number of the UV protection sheet for the Magelis HMIGTO2300, HMIGTO2310, and HMIGTO2315?


Product Line
Magelis HMIGTO2300, HMIGTO2310, HMIGTO2315
 

Environment
Direct sunlight
 

Resolution

The part number for the UV protection sheet for the HMIGTO2300, HMIGTO2310, and HMIGTO2315 5.7inch touchscreen panels is: HMIZG62

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.