Browse FAQs

What can cause an ILF [Internal Link Error] on an ATV340 series drive and how do I correct it?

Published date: 01 March 2019

Issue:
Customer is experiencing an ILF [Internal Link error] fault on an ATV340 series drives.

Product Line:
ATV340

Environment:
All

Cause:
Communication interruption between option module and the drive.

Resolution:
 Verify the environment (electromagnetic compatibility).
 Verify the connections.
 Replace the option module.
 Contact your local Schneider Electric representative


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.