Browse FAQs

Getting error "Volume is dirty" in SoMachine

Published date: 28 February 2019

Issue:
Getting error "Volume is dirty" in SoMachine

Product Line:
SoMachine V4.3

Resolution:
This is a message triggered by the OS or any component of the OS, and not SoMachine. 
If the customer builds the application or tries to login in, data (compileinfo file and so on) will be written into the folder where the project file is located. 
If there is a problem with the hard disk, such message could appear. 
Some information about this issue can be found online: 
https://ugetfix.com/ask/how-to-fix-0x80071ac3-the-volume-is-dirty-error-on-windows/ 
https://support.wdc.com/knowledgebase/answer.aspx?ID=15094&lang=en 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.