Browse FAQs

Can the shielding kit BMXXSP0800 be used for the redundant backplanes BMEXBP0602 and BMEXBP1002?

Published date: 22 February 2019

Issue
Which shielding kits can be used with the redundant X80 backplanes?

Product line
Modicon M580, Modicon X80

Resolution
The BMEXBP0602 would use the BMXXSP0800 kit.
The BMEXBP1002 would use the BMXXSP1200 kit.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.