Browse FAQs

Do any of the Altivar Process drives have any silicone on the boards terminals etc?

Published date: 22 February 2019

Issue:
Do any of the Altivar Process drives have any silicone on the boards terminals etc?

Product Line:
ATV320, ATV340 ATV600 and ATV900

Environment:
All 

Cause:
Silicone material in the drives

Resolution:
Most of our drives have Silicone in the power modules. This Silicone is partially encapsulated in the modules and therefore very weakly volatile.
In addition, there is a small percentage of silicone in the thermal grease under the modules.
Also some wire-pass insulator can be Silicone but with a zero risk of volatility.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.