Browse FAQs

Can the S-Flex212 be ordered with the Surge Protective Devices UL1449?

Published date: 22 February 2019

 Issue:
Needs a  S-Flex212  ordered with the Surge Protective Devices that are  UL1449? approved.

Product Line:
S-Flex 212

Environment:
All

Cause:
Customer needed to have inherent surge suppression in the SFlex.

Resolution:
No, the S-Flex does not have the surge protective device option.  Customer would have to order the ATV660, or contact Drive Quotation to see if they would quote SPD as a special. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.