Browse FAQs

In the product description of the 140CPU65260, what does the 4096/7168K represent?

Published date: 20 February 2019

Issue:
In the product description of the 140CPU65260, what does the 4096/7168K represent?

Product Line:
Modicon Quantum PLC

Resolution:
The 4096K represents the amount of physical memory that the Quantum Processor contains. The 7168K is the amount of expandable memory the the Quantum Processor can have.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.