Browse FAQs

Can the 140CRA31908 interface be used with M580 Safety PLC's?

Published date: 20 February 2019

Yes, the 140CRA31908 can be used with the M580 Safety PLC's. The S908 network created with the 140CRA31908 will not be part of the safety loop.
The safety loop will require use of BMX Safety IO and non-interfering BMX IO on the ERIO network.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.