Browse FAQs

How can you read KW over bacnet on the ATV61 drive with the Bacnet option card installed?

Published date: 26 February 2019

Issue:
Read KW over bacnet on the ATV61 drive.

Product Line:
ATV61 with Bacnet 

Environment:
All 

Cause:
KW reading over Bacnet 

Resolution:
Assign address value for OPRP or address 3227 to the input scanner table #3  in menu communications menu 1.9.
Now you can read analog output point #38 which will give you the value of the scanner table #3. 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.