Browse FAQs

Does the ATV630 have the capability of IEC 61131 programming?

Published date: 15 February 2019

Issue:
Does the ATV630 have the capability of IEC 61131 programming?

Product Line:
Altivar 630

Environment:
All

Cause:
Programming

Resolution:
IEC 61131 is a PLC standard. You would need to program a PLC using SoMachine, and SoMachine has function blocks that conform to IEC 61131-3.




Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.