Browse FAQs

How many I/O extension modules (cards) can be installed on the ATV630 ?  

Published date: 15 February 2019

Issue: 
Can I install (2) I/O extension modules a VW3A3202 Digital and analog module and a VW3A3203 Relay output module? 

Product Line: 
ATV630 

Environment
All serial numbers

Cause:
Need additional outputs digital and relays

Resolution
Yes, 2 I/O extension modules can be used if they are different part numbers.
(Note: You can not use two of the same I/O part numbers)
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.