Browse FAQs

Preventa XCS - Which product uses the ZCKE70 head and how to replace

Published date: 11 February 2019

The ZCKE70 head is used on the obsolete red switch body XCKJ59 or XCKJ79. Complete assembly is XCKJ5970 or XCKJ7970 (see attached picture). The XCKJ5970 obsolete reference can be replaced (same function) by the XCSA501 or XCSA502 (NC+2NO contacts) or XCSA701 or XCSA702 (2NC+NO contacts). The XCKJ7970 obsolete reference can be replaced (same function) by the XCSA701 or XCSA702 (2NC+NO contacts). Operating key has to be substituted.

Was this helpful?

What can we do to improve the information ?