Browse FAQs

How can you search for a specific parameter code in the Process drive using somove?

Published date: 07 February 2019

Issue:
How can you search for a specific parameter code in the Process drive using somove?

Product Line:
Somove Process drive

Environment:
All 

Cause:
Needs to filter the search results. 

Resolution:
If you need to only search for a specific code in the Drive you need to first 
Click the Parameters List TAB
Double click or highlight Drive in the upper left corner 
Type in the code that you want to search in the search bar... Example is BRA
Change ALL to Code in the next drop down selection 
Now Search
Now Code BRA comes up in the Drives parameter list. 



 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.