Browse FAQs

How to program an ATV320 drive to send feedback of motor frequency using the analog output?

Published date: 04 February 2019

Issue:
How to program an ATV320 drive to send feedback of motor frequency using the analog output?

Product Line:
ATV340, Altivar 340

Environment:
All

Cause:
NA

Resolution:
Go to Complete Settings, Input/Output, AI/AQ, AQ1 Configuration.
AQ1 assignment will need to be set for Motor Frequency (OFr).
AQ1T for type (Current or Voltage)
AQ1 min for min value such as 0mA or 4mA.
AQ1 max for 10V or 20 mA.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.