Browse FAQs

How to transfer cfg.file to Altivar Drive using the multi-loader ?

Published date: 28 February 2019

Issue:
How to transfer cfg.file to Altivar Drive using the multi-loader ?

Product Line:
VW3A8121

Environment:
All

Cause:
Needs to transfer a CFG file to Altivar Drive

Resolution:

Procedure is as follows:

>put the cfg file (ex.: test.cfg) to Multiloader's SD card

>connect Multiloader to ATV Drive

>turn-ON the multiloader

.wait...
..on the display:
Main Menu
Action

>press  [ENT]

..on the display:
Action Config
MLD->Device

>press [ENT]

.wait...
..on the display:
MLD -> Device
Folder or File name (1st file or folder will be displayed on this line)

>use arrows v^ to navigate and find the correct folder
>use [ENT] to enter the folder
>use v^ to select the correct cfg file (ex.: test.cfg)

..on the display:
MLD->Device
test.cfg

>press [ENT]

.wait...
..on the display:
test.cfg
>>>>>     (progress bar is growing left)

..on the display:
Store config
Successful

>press [ENT]

..on the display:
Action Config
MLD->Device

>turn-Off the Multiloader

>disconnect Multiloader from ATV Drive

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.