Browse FAQs

9007B - 9007BD10 cross-reference

Published date: 01 February 2019

9007BD10 cross-reference or replacement : XCKJ105 (ZCKJ1+ZCKE05) or ZCKJ1H29 + ZCKE05 or XCKJ1051H7 limit switch without lever arm. 9007BD10 is an obsolete IEC limit switch, industrial format EN 50041 standard. Lever arm has to be ordered separately in the ZCKY* range in the XCKJ spare parts

Was this helpful?

What can we do to improve the information ?