Browse FAQs

What timers are available in PM2125 meter ?

Published date: 28 June 2019

The meter supports an active load timer, meter operation timer, and run hour. The timer data can be read through register map.

Active load timer
Active load timer shows how much time a load has been running, based on the specified minimum current for the load timer setpoint setting.

Meter operation timer
Meter operating timer shows how long the meter has been powered up.

Run Time
Run time shows how much time a load has been running, based on accumulated energy - received and delivered.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.