Browse FAQs

What is the function of AU4 parameter of the ATV212 drive?

Published date: 27 June 2019

 Issue:
Function of AU4 parameter of the ATV212 drive.

Product Line:
Altivar ATV212

Environment:
All serial numbers

Cause:
N/A

Resolution:
The ATV212 drive can be configured for four common control programs by setting parameter AU4.  Please see the attachment below for detail or on page 67 in the ATV212 programming manual, document number S1A53838 (https://www.schneider-electric.us/en/download/document/S1A53838/).


 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.