Browse FAQs

ATV660- what is the default password of the Zelio relay?

Published date: 29 January 2019

Issue:
 On the ATV660 enclosed package, what is the default password of the Zelio relay?

Product Line:
ATV660 

Environment:
Zelio relay

Cause:
n/a

Resolution:

The default password from the factory is 6601. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.