Browse FAQs

What version of Rockwell RSLogix5000 .L5K files are supported for Symbol Link in Vijeo XD v3.0?

Published date: 28 January 2019

Issue
What version of Rockwell RSLogix5000 .L5K files are supported for Symbol Link in Vijeo XD v3.0?

Product Line
Vijeo XD v3.0

Environment
Windows PC Configuration Software

Resolution
Rockwell RSLogix5000 .L5K symbol files that are supported in Vijeo XD v3.0 are:
version 13, 15, 16, 17, 18, 19, 20, and 21

Note:  FS, LS, OV, and ER of TIMER Predefined types are not supported.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.