Browse FAQs

Osisense XC - Where are indicated the commercial ref. and the manufacture date on the XCKM switch body

Published date: 28 January 2019

On the XCKM limit switch bodies, the commercial reference and the manufacture date are indicated on the product label sticked on case side, or marked on the front cover. The manufacture date, or date code, is indicated like that : Plant code - Year - Week. Please have a look at the attached picture example, showing a ZCKM1H29 switch body.

Was this helpful?

What can we do to improve the information ?