Browse FAQs

How do I avoid the message "Cannot set Two-Way converter. Change converter mode or Enable User Input." for Numeric Displays in Vijeo XD v3.0?

Published date: 25 January 2019

Issue
In Vijeo XD v3.0, I am getting a "Cannot set Two-Way converter. Change converter mode or Enable User Input." build message even if I don't use Value Conversion on a screen object and I cannot build my project. How do I get past it?

Product Line
EcoStruxure Operator Terminal Expert (Vijeo XD) v3.0

Environment
Windows Application for HMI Configuration

Resolution
To resolve the message, 
1) Double-click the message. This will select the screen object.
2) In the screen object, the Variable field in question should be highlighted with Red or Orange
3) Click the button to the right of the Variable name and choose "Variable" to open the variable selection screen
4) Select "One-Way" Converter instead of "Two-Way" next to "Direction"
5)Accept the changes with the OK button

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.