Browse FAQs

When assigning an ATV32 function, why does the assignment option only show COMP?

Published date: 24 January 2019

Issue:
When assigning an ATV32 function, why does the assignment option only show COMP?

Product Line:
ATV32

Environment:
All models

Cause:
Attempting to assign an ATV32 function, but COMP is shown instead of normal options.

Resolution:
This indicates that this function in incompatible with another function that is already assigned.
See attachment for info.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.