Browse FAQs

What are the specifications for the LTME expansion modules?

Published date: 23 January 2019

Issue:
What are the specifications for the LTME expansion modules?

Product Line:
Tesys T

Environment:
All

Cause:
N/A

Resolution:
2 options: LTMEV40BD (24VDC) and LTMEV40FM( 100...240VAC)
  • voltage sensing 110...690Vac
  • 3-phase voltage inputs
  • 4 additional discrete logic inputs
  • additional voltage protection, metering and monitoring functions
  • power LED indicator
  • logic input status LED indicators
  • LTMR controller to LTME connection cable needed.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.