Browse FAQs

What are the specifications for the LMTR controllers?

Published date: 23 January 2019

Issue:
What are the specifications for the LMTR controllers?

Product Line:
Tesyst

Environment:
All

Cause:
N/A

Resolution:
Functional description:
  • current sensing 0.4...100A
  • single-phase or 3-phase current inputs
  • 6 discrete logic inputs
  • 4 relay outputs: 3 SPST, 1 DPST
  • connections for a ground sensor current
  • connection for a motor temperature sensor
  • connection for network
  • connection for HMI device or expansion module
  • current protection, metering and monitoring functions
  • motor control functions
  • power indicator
  • fault and warning LED indicators
  • network communication and alarm indicators
  • HMI communication LED indicator
  • test and reset function

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.