Browse FAQs

Does Intelligent Data Services (IDS) need to have a registered Vijeo Designer Runtime PC License to run on HMIG5U or HMIG5U2?

Published date: 21 January 2019

Issue
Does Intelligent Data Services (IDS) need to have a registered Vijeo Designer Runtime PC License to run on HMIG5U or HMIG5U2?

Product Line
Vijeo Designer v6.2, Intelligent Data Services (IDS), Magelis OPEN Box HMIG5U, Magelis OPEN Box HMIG5U2

Environment
Windows PC, Magelis OPEN Box HMIG5U, Magelis OPEN Box HMIG5U2

Resolution
No. There is no such restriction for the Magelis HMIG5U or HMIG5U2. As long as Vijeo Designer Runtime is installed on the HMIG5U/HMIG5U2, a registered version of Intelligent Data Services (IDS) will run continuously without stopping after 2hours.

However, on a Windows PC (Magelis iPC or 3rd-party Standard PC that is not HMIG5U or HMIG5U2) without a purchased and registered Vijeo Designer Runtime PC License, Intelligent Data Services (IDS) will give a popup message upon launch that it will only run for a 2h trial period before it needs to be re-launched. This is true on all Magelis iPCs and Standard PCs if Vijeo Designer Runtime is not registered.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.