Browse FAQs

Is there a difference between the terms Connected vs Device Connected in Management Console?

Published date: 29 January 2019

Issue
Is there a difference between the terms Connected vs Device Connected in Management Console?

Product Line
Power Monitoring Expert

Environment
Management Console

Cause
In PME, when view the Management Console application, the Status of a device is seen as Connected and/or Device connected. Is the a difference between the meaning?

Resolution
Both these terms, 'Connected' and 'Device Connected', mean the same and are used interchangeable. There was a change in an earlier software version and since it's been hard-coded into the software that's why both terms are seen in Management Console.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.